Education Technology

Knowledge Base

Home | Financial Calculators

Solution 11244: Depreciation Worksheet on the BA II PLUS™ Family Calculator.

How do I use the depreciation worksheet on the BA II PLUS family calculator?

The following example demonstrates how to use a depreciation worksheet on a BA II PLUS family calculator. 

Example: In the beginning of January, a company begins to depreciate a machine with a 7 year life and no (0) salvage value. The machine costs $300,000. The declining balance percent is 200.

1) Press [2nd] [Depr] to enter the Depreciation worksheet 
2) Press [2nd] [CLR Work] to clear the worksheet 
3) If necessary, press [2nd] [SET] until DBX appears in the display to select declining-balance crossover method
4) Input 200 and press [ENTER] to input the declining balance percent (ENTER is located to the right of CPT) 
5) Press the down arrow once, then input 7, and press [ENTER] to enter the life in years 
6) Press the down arrow once, then input 1, and press [ENTER] to enter the starting month 
7) Press the down arrow once, then input 300000, and press [ENTER] to enter the cost 
8) Press the down arrow once and make sure SAL (salvage value) is set to 0 
9) Press the down arrow once and make sure YR is set to 1 
10) Press the down arrow once and the depreciation amount (DEP) for the first year is shown, which is $85,714.29 
11) Press the down arrow once and the remaining book value (RBV) for the first year is shown, which is $214,285.71 
12) Press the down arrow once and the remaining depreciation value (RDV) for the first year is shown, which is $214,285.71 
13) Press the down arrow once and press [CPT] to compute DEP, RBV, and RDV for the second year. Repeat the step above in order to compute the remaining years.

For more information, please see the BA II PLUS family guidebook.