Solution 16309: Details Surrounding the VST Apps Calculator Program from Vernier Software & Technology.
What are the details surrounding the VST Apps Calculator Program from Vernier Software & Technology?
The VST App is an application that performs specialized data collection with the TI-83 Plus, TI-84 Plus family, LabPro and CBL 2™ devices. It is a wrapped application that includes the following specialty programs:• DataMatch:
Used with the Motion Detector. The program presents distance vs. time and velocity vs. time graphs, and challenges students to match the graph.
• DataGate:
Used to collect data with photogates or Smart Pulleys™.
• DataRad:
Used with the Student Radiation Monitor and the Radiation Monitor to monitor nuclear radiation. A variety of data collection modes are supported.
• DataRotary:
Used with the Vernier,
• DataDrop:
Used with the Vernier Drop Counter. It is useful for automating titration or equivalence point experiments.
• FunctGen:
Allows the calculator to command a LabPro interface to behave like an analog function generator. This program only works with LabPro and requires LabPro operating system 6.22.
Note: None of these program can be loaded into the RAM of the calculator. If the program was previously installed on the calculator as a standalone program, delete it before using the VST Apps application.