Education Technology

Algebra II: Stacking Bricks - 84

by Texas Instruments

About the Lesson

Students start by determining the number of bricks in a stack with 1, 2, 3, 4, 5, and 6 rows. Then they will calculate the successive differences and record the values in the table on the worksheet. Students also need to enter the data for L1 and L2 in the calculator. Then, they use the QuadReg command from the Calc menu. Explain to students that when they enter L1, L2, Y1 after the command, this tells the calculator that the x-values they want to model are in L1, the y-values are in L2, and the equation for the model should be stored in Y1. Finally, students will compare the model to the data by creating a scatter plot. The graph screen should appear as shown at the right with the line passing through all of the points.