Education Technology

Inequalities, They Are Not Just Linear Anymore!

Subject Area
Math: Algebra I: Equations and Inequalities
Level
9-12
Activity Time
90 Minutes
Software
TI Connect™
TI Calculator
TI-84 series
Other Materials
This is Activity 6 from the EXPLORATIONS Book:
Exploring Mathematics with the Inequality Graphing Application

Inequalities, They Are Not Just Linear Anymore!

Activity Overview

Students study quadratic relationships and explore the process of graphing quadratic inequalities and systems of quadratic inequalities. They will solve these inequalities algebraically and graph them on a coordinate plane.

Before the Activity

Install the Inequality Graphing Application on the calculator using one of these two methods:

  • TI Connect™, a TI Connectivity Cable, and the Unit-to-Unit Link Cable
  • TI-Navigator™ "send to class" feature

See the attached PDF file for detailed instructions for this activity
Print pages 59-67 from the attached PDF file for your class

During the Activity

Distribute the pages to your class.

Follow the Activity procedures:

  • Graph the equation y = x2
  • Locate points and algebraically determine if they are part of the solution set of the inequality y > x2
  • Observe that all the points that are part of the solution set lie inside the parabola y = x2
  • Use the Inequality Graphing Application to graph the inequality and verify the observation
  • Graph a system of quadratic inequalities
  • Predict if the two inequalities intersect in one or more points
  • Use the Inequality Graphing application to verify the prediction
  • Use the Inequality Graphing application to graph another system of quadratic inequalities

After the Activity

Students will complete the Student Worksheet and answer questions.

Review student results:

  • As a class, discuss questions that appeared to be more challenging
  • Re-teach concepts as necessary
  • Subject Area
    Math: Algebra I: Equations and Inequalities
    Level
    9-12
    Activity Time
    90 Minutes
    Software
    TI Connect™
    TI Calculator
    TI-84 series
    Other Materials
    This is Activity 6 from the EXPLORATIONS Book:
    Exploring Mathematics with the Inequality Graphing Application

    iPad is a trademark of Apple Inc., registered in the U.S. and other countries.
    Vernier EasyData,Vernier EasyLink and Vernier EasyTemp are registered trademarks of Vernier Science Education.