Education Technology

Knowledge Base

Home | TI-Nspire™ Navigator

Solution 37697: Mismatch between number of clients reported by the TI-Nspire™ CX Navigator software and the number of clients actually connected to the system.

Why is there a mismatch between number of clients reported by the TI-Nspire CX Navigator™ software and the number of clients actually connected to the system during setup?

After performing the system setup of a wireless TI-Nspire CX Navigator class set, there is a mismatch between number of clients reported by application and the number of clients actually connected to the system.

This issue can happen during wireless setup using the setup wizard. Please close and relaunch the software or change the access point channel/disconnect reconnect the access point.