Education Technology

Knowledge Base

Home | TI-Innovator™ Technology

Solution 38056: TI-Innovator™ Hub Inconsistent readings between Grove DHT11 and DHT22 Sensors.

Why does the TI-Innovator Hub give inconsistent readings between Grove DHT11 and DHT22 Sensors?

Grove has two different digital humidity and temperature sensors DHT11 and DHT22.

The two sensors result in different readings even when used in the same setup.

This is a general issue with Grove sensors as they are not high-precision sensors and have piece-to-piece variation.