Solution 21049: Entering and Computing Fractions on the TI-83 Family, TI-84 Plus Family, or TI-Nspire™ Handheld in TI-84 Plus Mode.
How do I enter and compute fraction problems on a TI-83 family, TI-84 Plus family, or TI-Nspire handheld in TI-84 Plus Mode?
The TI-83 family, TI-84 Plus family, or TI-Nspire handheld in TI-84 Plus Mode are not fraction calculators and do not have a specific fraction key. The TI-84 Plus family and TI-Nspire in TI-84 Plus mode do have a template that allows fractions to be entered. On the TI-83 family use the division key [/].
Before beginning, ensure that you have the latest Operating System, by visiting the Software and OS Updates page.
For example, using the TI-84 Plus or TI-Nspire in TI-84 Plus mode, add 3 2/5 to 3/4 using the steps below:
• Press [ALPHA] [F1] [1]
• Enter in [3] and scroll
• Scroll down
• Enter in [4]
• Scroll to the right
• Press [+]
• Press [ALPHA] [F1] [2]
• Enter in [3]
• Scroll to the right
• Enter in [2]
• Scroll down
• Enter in [5]
• Press [ENTER]
• Depending on settings, below are two possible answers with MATHPRINT turned on and switching from n/d to Un/d.
For the TI-83 family please see the below example.
Example: (5 8/13) / (9/23)
• Press [(] [5] [+] [8] [/] [1] [3] [)]
• Press [/]
• Press [(] [9] [/] [2] [3] [)]
• Press the [MATH] [1]
• Press the [ENTER]
NOTE: This may also be done on the TI-84 Plus and TI-Nspire in TI-84 Plus mode.
Changing a decimal into a fraction.
Example: Convert .4 into a fraction
• Press [.] [4] [MATH] [1] [ENTER]
Changing a fraction into a decimal.
Example: Convert 15/6 into a decimal
On the TI-84 Plus or TI-Nspire in TI-84 Plus mode:
• Press [MODE]
• Scroll up four times or scroll down ten times to get to ANSWERS
• Scroll to the right
• Press [ENTER] [2nd] [QUIT]
• Press [ALPHA] [F1] [1]
• Enter in [1] [5]
• Scroll down
• Press [6] [ENTER]
On either TI-83 family, TI-84 Plus family, or TI-Nspire in TI-84 Plus:
• Press [1] [5] [/] [6] [ENTER]
Please see the TI-83 family and TI-84 Plus family guidebooks for additional information.
NOTE: TI-Nspire users may refer to the TI-84 Plus family guidebook.