Education Technology

Solution 11757: Finding the X-Intercepts of a Function Using the TI-83 Family, TI-84 Plus Family and TI-Nspire™ Handheld in TI-84 Plus Mode.

How can I find the x-intercepts of a function using a TI-83 family, TI-84 Plus family and TI-Nspire Handheld in TI-84 Plus mode?

To find the x-intercepts of a function using a TI-83 family, TI-84 Plus family and TI-Nspire Handheld in TI-84 Plus mode, the zero command must be used. Follow the example below for help with using the zero command.

Example function: 2X - 7

1) Press the [Y=] key to access the Y= Editor.
2) For Y1=, input the example function. Press the [GRAPH] key to graph the function.

3) To use the zero command, press [2nd] [TRACE] to access the CALC menu, then press [2] to select the zero command.
4) The handheld will then prompt for a "Left Bound". This means the handheld wants the user to select a point on the graph that is to the left of the x-intercept. Using the arrow keys, move the cursor until it is to the left of the x-intercept. Press [ENTER] to mark this as the left bound.

5) The handheld will then prompt for a "Right Bound". This means the handheld wants the user to select a point on the graph that is to the right of the x-intercept. Using the arrow keys, move the cursor until it is to the right of the x-intercept. Press [ENTER] to mark this as the right bound.

6) The handheld will then prompt for a "Guess". This means the handheld wants the user to take a guess at the x-intercept. Using the arrow keys, move the cursor until it is close to or directly on the x-intercept. Press [ENTER] to mark this as the guess. This will also complete the zero command and display the exact point of the x-intercept which is (3.5,0).

Please see the TI-83 family and TI-84 Plus family guidebooks for additional information.