Education Technology

Solution 16269: Copying a TI-SmartView™ Emulator Software Script to Another Application.

How can I copy a TI-SmartView script to another application?

It is possible to copy all or only a selected portion of a script to another application such as a word processor. It is possible to copy the key graphics as they are shown in the script pane, or the key presses can be copied as font text characters.

Note: When copying as font text characters, those characters use the TI84EmuKeys font. This font is automatically installed on the computer with the emulator software.

To copy keys as graphics:

• Open the appropriate script.

• Select the keys to be copied. To select all the keys, click Edit >Select All.

• Click Edit > Copy, switch to the other application, and paste the keys at the appropriate location.

Note: Another possibility is to drag the selected keys to the new application.

To copy keys as font text characters:

 • Open the appropriate script.

 • Select the keys to be copied. To select all the keys, click Edit >Select All.

 • Click Edit > Copy As Font.

 • Switch to the other application, and paste the characters at the appropriate location.

In some applications, the pasted characters may be shown in the font that is in effect at that location. So they may not look anything like calculator keys. If necessary, apply the TI84EmuKeys font to the characters.

Note: The script icons for text points, delays, pauses, and Go To Home commands cannot be copied as font text characters. They are ignored when pasted into the other application.

Please see the TI-SmartView guidebooks for additional information.