Education Technology

Solution 11466: Using the TI-SmartView™ Emulator Software with the Computer Keyboard.

Can I use the computer keyboard to type commands in the TI-SmartView emulator software?

The computer keyboard can be used only for shortcuts. The keyboard cannot be used to enter plain text. For example, to enter a file name for a program, click the appropriate keys on the calculator. If the file name contains letters, the [ALPHA] key must be used plus another key for each letter.

A keyboard shortcut lets you press a key on the keyboard instead of using the mouse to click a key on the calculator.

Keyboard shortcuts for calculator keys are as follows.

If you have questions about the information listed above please contact TI-Cares for additional assistance.