Education Technology

Solution 34292: Using the Percent Key on the TI-36X Pro.

How do I use the percent key on the TI-36X Pro?

The example below will demonstrate using the percent key in an operation on the TI-36X Pro.

Example: What is 50% of 100?

• Input 50.
• Press [2nd] [%].
• Input 100 and press [enter].

The calculator should display 50 as the solution.

Please see the TI-36X Pro guidebook for additional information.