Knowledge Base
Solution 33891: Calculating the Determinant of a Matrix Using a TI-36X Pro.
How do I calculate the determinant of a matrix using a TI-36X Pro?
The instructions below will demonstrate how to find the determinant of a matrix using a TI-36X Pro.For Example: What is the determinant of matrix A?

To enter the matrix, please follow the steps below:
1) Press [2nd] [matrix].
2) Scroll to EDIT and press [enter].
3) Select 2 for ROWS and 2 for COLUMNS.
4) Scroll to OK and press [enter].
5) Press [4] [enter] [(-)] [1] [enter] [(-)] [3] enter] [2] [enter].
6) Exit the matrix editor by selecting [2nd] [quit].
To find the Determinant using the function:
7) Press [2nd] [matrix].
8) Scroll to MATH.
9) Press 1: Determinant.
10) Press [2nd] [matrix].
11) Under NAMES, press 1: [A] 2x2.
12) Press [enter] to display the answer of 5.
Please see the TI-36X Pro guidebook for additional information.