Education Technology

Solution 20269: Computing nth Roots Using the TI-30XS/B MultiView™ or TI-34 MultiView™ Scientific Calculators.

How do I compute nth roots using the TI-30XS/B MultiView or TI-34 MultiView scientific calculator?

To compute nth roots using the TI-30XS/B MultiView or TI-34 MultiView scientific calculators, please follow the below example:

Example: What is the cubed root of 27?

Solution:

1) Input 3 and press [2nd] [^]. This will input the nth root function with the value of 3 as the degree.

2) Input 27 and press [enter].

The display should read 3.

Please see the TI-30XS/B MultiView and TI-34 MultiView guidebooks for additional information.