Education Technology

Solution 12238: Clearing a Stored Operation on the TI-15 Explorer™.

How can a stored operation be cleared on the TI-15 Explorer?

The following keystrokes will clear a selected stored operation on the TI-15 Explorer:


• Press [Mode] [▼] [▼].
• The display will read "OP1 CLEAR OP2".
• Use either [◄] or [►] to select an operation.
• With the cursor under the operation that is to be cleared, press [Enter].

The selected "OP" indicator should disappear from the display.

More information on how to use the TI-15 Explorer calculator can be found in the TI-15 Quick Reference Guide.