Knowledge Base
Solution 10696: Replacing The Battery in a TI-36X II.
What type of battery is used in the TI-36X II and how is it installed?
About replacing the button cell battery on a TI-36X II Scientific
calculator:
For safety purposes and to prevent ingestion, the
button-cell batteries in school- and student-owned calculators without battery
doors are not designed to be replaced. It is possible to replace the battery by
removing the back case of the calculator, but opening the back of the calculator
voids the one-year, limited warranty. This must be done carefully, as we cannot
be held responsible for any damage caused when you attempt to replace the
battery. If your calculator is already out of warranty, you might
choose to remove the back case to replace the battery.
To replace
the battery:
1) Remove the screw case, using a small Phillips®
screwdriver.
2) Carefully separate front from back, starting from the bottom.
Caution: Be careful not to damage
any internal parts.
3) Remove battery, using a small Phillips screwdriver if
necessary; replace the old battery with the new battery. Install battery
according to polarity (+ and -) diagrams.
Caution: Avoid contact with other TI-36X II
components while changing the battery.
If necessary, press ON and CLEAR
simultaneously to reset. When released, memory and settings are cleared and MEM
CLEARED is displayed.
Properly dispose of the used battery
immediately.