Education Technology

Solution 10375: Correcting a DOMAIN Error When Using the Seq() Command on the TI-82.

Why do I get a DOMAIN Error when using seq() command on the TI-82?

A DOMAIN Error is returned when a list generated by the seq() command has more than 99 elements, which is the most elements the TI-82 will hold. The range or step of the seq() command will need to be adjusted so the list has at most 99 elements.

Please see the TI-82 guidebook for additional information.