Education Technology

Solution 28930: Restoring the Preloaded Apps on the TI-89 Family, TI-92 Plus, and Voyage™ 200 Using the TI Connect™ Software for Mac®

I accidentally deleted the pre-loaded apps from my TI-89 Titanium calculator; how can I restore them using the TI Connect software for Mac®?

To restore the pre-loaded apps on the TI-89 family, TI-92 Plus, or Voyage 200 calculator using the TI Connect software for Mac®, follow the steps below. If the TI Connect software for Mac® is not installed on the computer, download it from TI Connect software home page.

• With the TI Connect for Mac® software installed and the calculator connected to the computer, open the TI Device Explorer by going to Mac Hard Drive > Applications > TI Connect > TI Device Explorer.
• If the TI Device Explorer detects the connected calculator, the model number of the calculator will be displayed at the top of the window.
• If using a TI-89 calculator, download and save the "89 (pre-loaded).zip" file to the computer's desktop. If using the TI-89 Titanium calculator, download and save the "89 Titanium (pre-loaded).zip" file. If using a TI-92 Plus calculator, download and save the "92 Plus (pre-loaded).zip" file. If using the Voyage 200 calculator, download and save the "Voyage 200 pre-loaded).zip" file.
• Double-click on the .zip file to "unzip" it.
• With the .zip file unzipped, highlight all of the calculator app files and drag and drop them into the TI Device Explorer window. This should start the pre-loaded apps restore process.

For additional information on using the TI Connect for Mac® software, open the software by going to Mac Hard Drive > Applications > TI Connect > TI Connect X, click on the "Help" menu and select "TI Connect X Help".