Education Technology

Solution 12130: Difference Between the FIX and FLOAT Display Digits Mode Settings on the TI-89 Family, TI-92 Family and Voyage™ 200 Graphing Calculators.

What is the difference between the FIX and FLOAT Display Digits mode settings on the TI-89 Family, TI-92 Family and Voyage 200?

By default, the Display Digits mode setting is FLOAT 6, which means that results are rounded to a maximum of six digits. The [MODE] key can be used to select different settings which will apply to all exponential formats.

Internally, the device calculates and retains all decimal results with up to 14 significant digits (although a maximum of 12 are displayed).

Setting 

 Example

Description 

FIX
(0-12)

123.         (FIX 0)
123.5       (FIX 1)
123.46     (FIX 2)
123.457   (FIX 3)

Results are rounded to the selected number of decimal places.

FLOAT

123.456789012 

Number of decimal places varies, depending on the result.

FLOAT
(1-12)

1.E2        (FLOAT 1)
1.2E2      (FLOAT 2)
123         (FLOAT 3)
123.5      (FLOAT 4)
123.46    (FLOAT 5)
123.457  (FLOAT 6) 

Results are rounded to the total number of selected digits.


Note:
Regardless of the Display Digits setting, the full value is used for internal floating-point calculations to ensure maximum accuracy.

Note: A result is automatically shown in scientific notation if its magnitude cannot be displayed in the selected number of digits.

For additional information on mode settings, refer to the online guidebook for your specific calculator model.