Education Technology

Knowledge Base

Home | Financial Calculators

Solution 11222: Calculating Multiple Internal Rate of Return (IRR) Solutions on the BA II PLUS™ and the BA II PLUS PROFESSIONAL.

How are multiple Internal Rate of Return (IRR) solutions calculated on the BA II PLUS or the BA II PLUS PROFESSIONAL?

When a sequence of cash flows has two or more sign changes, there may be more than one solution for Internal Rate of Return (IRR).

In cases where there is more than one solution, the BA II PLUS and the BA II PLUS PROFESSIONAL will display the solution that is closest to zero. However, the displayed solution has no financial meaning.

For more information please check the BA II PLUS or BA II PLUS PROFESSIONAL guidebook.