Education Technology

Knowledge Base

Home | Data Collection

Solution 11191: Availability of Presentation Link Adapters.

What are the details surrounding Presentation Link adapters?

The Presentation Link is packaged with the TI-84 Plus Silver Edition ViewScreen™ Package, TI-89 Titanium ViewScreen Package, and sold separately. The Presentation Link adapters can be purchased from the TI Online Store.

The Presentation Link adapters are used on student TI-84 Plus family and TI-89 Titanium calculators to connect to the TI-Presenter™, and ViewScreen Panels.

To connect the Presentation Link adapter, firmly plug the connector on the ViewScreen panel cable, or the TI-Presenter video adapter cable into the port on the Presentation Link until it snaps into place. Next, push the USB connector on the Presentation Link cable straight into the USB port on top of the calculator device.