Solution 33091: Configuring the TI-Navigator™ (Nav-AP-US) Access Point for use in the TI-Navigator Classroom Network.
How do I configure the TI-Navigator (Nav-AP-US) Access Point for use in the TI-Navigator Classroom Network?
Please follow the steps below to configure the TI-Navigator (Nav-AP-US) Access Point for use in the TI-Navigator Classroom Network:
Please Note: The steps below only correspond to Type I and Type II Access Points pictured below. For assistance with the Nav-AP-US Access Point please visit Knowledgebase Article #31211.
• First open TI-Navigator Network Manager by clicking [Tools] [Network Manager] from within the TI-Navigator Software.
• Connect the TI-Navigator Access Point to a power source using the supplied AC Adapter and connect the Access Point to the computer using the supplied USB cable.
• Next to verify if the Access Point is listed as [Connected] or [Detected] as shown in the image below.
If you need additional assistance with other components of the TI-Navigator System please visit Knowledgebase Article #31211.
If you need assistance with any of the steps listed above or if the troubleshooting does not correct your issue please call the TI-Navigator support line at 1-866-846-2844 Monday-Thursday 8:00 AM - 7:00 PM and Friday 10:00 AM - 7:00 PM Central Standard Time or fill out the TI-Cares™ Customer Assistance Form.