Education Technology

Knowledge Base

Home | All other products

Solution 15121: Excluding a Selected Student's Answers Using the TI Navigator™ Class Analysis Software.

How can I exclude a selected student's answers using the TI-Navigator Class Analysis software?

Users can temporarily exclude a student's answers from a Class Analysis for "what if" purposes. Excluded students' answers are shown in italics and with a different background color than that of the other entries.

If the Class Summary tab is displayed:

• Click the Exclude check box next to the student's name to select it.

The student's responses are omitted from calculations and reports.

If the Student tab is displayed:

• Click the current Student to display the list of students, and then click the student whose answers are to be excluded.

• Click to select the Exclude Student from Analysis check box beneath the student's name.

The student's answers are excluded, and the analysis scores are recalculated. When ready to include the student's answers again, clear the Exclude check box.

Note: If the educator prefers, the student can be removed from the analysis.

If the Class Summary tab is displayed:

• Click the student's name

• Click Edit>Remove Student a dialog box should open.

• Click Yes to remove the selected student.

If the Student tab is displayed:

• Click Edit>Remove Student a dialog box should open.

• Click Yes to remove the selected student.


Please see the TI-Navigator documentation for additional information.