Activity Overview
Exploring the Depths with Uniform Motion is a project-based STEM activity that explores uniform motion and will engage your students in the engineering design process while using TI-Nspire™ technology. and the TI-Innovator™ Hub.
Objectives
Students will research science topics including:
- Uniform (non-accelerated) motion
- Change in position
- Speed
- Velocity
Vocabulary
- ROV (remote operation vehicle)
- Hoist
- Change in position
- Speed
- Velocity
- Y-intercept
- Slope
About the Lesson
Sonja Sonar is an ROV (Remote Operation Vehicle) mechanical engineer and has designed an ROV that can go deep into the ocean, in search of the elusive Giant Squid thought to live deep in the Marians trench. Presently, she has lost control of the ROV, which she believes has become stuck under a shelf in the canyon. To free the ROV, she needs to design a hoist to lower a search vehicle into the ocean to locate the stranded ROV and free it from its entanglement.
As a result, students will:
- Engineer and build a small hoist to raise or lower an object 1 vertical meter.
- Use mathematical processes of:
- Slope of a line
- Y-intercept of a line
- Interpreting graphs
- Proportional reasoning