Knowledge Base
Solution 11448: Creating a New Stack of Study Cards for Use with the StudyCards™ Application (App).
How can I create a new stack of study cards for the StudyCards App?
In order to create a new stack of study cards for the StudyCards App, the StudyCards Creator software will need to be installed on the PC.
NOTE: The StudyCards Creator software is not supported on Mac operating systems.
To create a new stack, follow the instructions provided below.
• Open
the StudyCards Creator software.
• Select the correct device type and the
type of stack to be created.
• Click OK to begin the
stack.
• Name the stack and fill in all the appropriate fields to create the
new stack and the first card of this stack.
• To add another card to the
stack, click the icon in the top toolbar that looks like a card with a big
yellow plus sign.
• Fill in all the appropriate fields to create the new
card.
• Add as many cards as desired.
• Once the stack is complete, choose
File in the top toolbar and select Save to
save this stack.
• To transfer the stack to the calculator, drag and drop the
stack file on top of the TI Connect™ icon.
• The new stack has been created
and transferred to the calculator.