Solution 18849: Not able to Clear the Screen of a New TI-503SV, TI-1706SV, or TI-1795SV Calculator.
What should I do if I have recently purchased a new TI-503SV, TI-1706SV, or TI-1795SV calculator and the screen will not clear?
Look very closely at the screen of the calculator, it may be very hard to see unless you are under direct sunlight but there is a sticker over the front of the calculator screen. There should be a tab located at the beginning of the sticker that will allow you to peel the sticker off so you can use it normally. This sticker found on the calculator is used for marketing purposes so it can be displayed at stores to show what the screen would look like if it is turned on.