Perimeter of a Rectangel with Fixed Area
9-12
Perimeter of a Rectangel with Fixed Area
Students will investigate the relationship between the base of a rectangle with area of 35 or 36 and its perimeter.
Prepare the Activity Center with the desired windows
0
Assign each pair of students one of the following numbers:
2, 3, 4, 5, 6, 7, 8, 9, 10, 12, 14, or 18. Have them draw a rectangle with that number for a base and having an area of 35 or 36.(or provide a worksheet with rectangles already drawn).
Have the students calculate (or measure) the height of the rectangle and its perimeter. The students can either enter their base and perimeter as a point to contribute to TI-Navigator™, or the teacher can call on students to randomly to submit their points to an overhead calculator.
Do a scatter plot of the data.
Talk about calculating the height by dividing 36 by the base. Take the perimeter formula and substitute x for the length and 36/x for the width in P= 2(l + w) to get P=2(x + 36/x).
Show that when you enter y=2(x+36/x) the line hits all of the points.
Ask the students to look at the graph and tell the minimum value for the perimeter.
During the Activity Files
9-12
Vernier EasyData,Vernier EasyLink and Vernier EasyTemp are registered trademarks of Vernier Science Education.