Meaning of Alpha
Math: Statistics: Hypothesis Tests
9-12
45 Minutes
TI-Nspire™ CX series
TI-Nspire™ CX CAS/CX II CAS
3.0
Lessons
TNS
Meaning of Alpha
Activity Overview
- Students will recognize that the alpha value (significance level of a test) is the relative frequency for sample statistic values that lead to a "reject the null" conclusion, given that the null hypothesis is actually true.
- Students will recognize that a sample mean can lead to a "reject the null" or "fail to reject the null" depending on the alpha level.
Objectives
- Students will recognize that the alpha value (significance level of a test) is the relative frequency for sample statistic values that lead to a “reject the null” conclusion, given that the null hypothesis is actually true.
- Students will recognize that a given sample mean can lead to a “reject the null” or “fail to reject the null” depending on the alpha level.
Vocabulary
- alpha level
- population
- samples
- sampling distributions of sample means
- significance level
About the Lesson
This lesson involves beginning with a null hypothesis specifying the mean of a normally distributed population with a given standard deviation.
As a result, students will:
- Generate a sample and sample mean and predict whether the sample might reasonably have come from the hypothsized population, considering the criteria they would use to make a decision.
- Consider a fixed alpha level (0.1) and predict the likelihood of getting by chance an outcome at least as extreme as the value determining the border of the rejection region if the null hypothesis is true.
- Generate 100 samples, and observe how many fall into the rejection region to observe that the decision to reject or not to reject the null hypothesis will change depending on alpha.

Download Files
Math: Statistics: Hypothesis Tests
9-12
45 Minutes
TI-Nspire™ CX series
TI-Nspire™ CX CAS/CX II CAS
3.0
Lessons
TNS
iPad is a trademark of Apple Inc., registered in the U.S. and other countries.
Vernier EasyData,Vernier EasyLink and Vernier EasyTemp are registered trademarks of Vernier Science Education.
Vernier EasyData,Vernier EasyLink and Vernier EasyTemp are registered trademarks of Vernier Science Education.