Matrix Transformations
Matrix Transformations
Grab vertices of a polygon undergoing reflections and rotations in the coordinate plane to determine the transformation’s type.
- Students will be able to identify the correct 2 x 2 matrix that, when multiplied to a matrix representation of a polygon, results in a polygon: • Reflected across the x-axis. • Reflected across the y-axis. • Rotated 90° about the origin. • Rotated 180° about the origin.
- rotation
- reflection
- matrix
- element
- identity
This lesson involves grabbing vertices of a polygon undergoing reflections and rotations in the coordinate plane to determine the transformation’s type. It also involves duplicating a reflection or rotation by: changing the elements of 2x2 matrices and evaluating the effects of the multiplying matrix on the polygon in the coordinate plane. As a result, students will make conjectures about the relationships between certain 2x2 matrices and their effects on the resulting transformed polygons obtained through matrix multiplication.
Vernier EasyData,Vernier EasyLink and Vernier EasyTemp are registered trademarks of Vernier Science Education.