Arc Length and Sectors
Arc Length and Sectors
Investigate the mathematics of arc length and sectors.
- Students will recognize that the sum of two central angles that combine to make a circle is 360°.
- Students will recognize that the ratio of the central angle to 360° determines the length of an arc.
- Students will recognize that the ratio of the central angle to 360° determines the area of a sector.
- circumference
- area
- arc
- sector angle (or central angle)
- arc measure
- arc length
- sector
This lesson involves dragging a point around a circle to see how arcs and sectors change as the central angle defining them changes. As a result, students will:
- Watch the central angles, sectors, and accompanying ratios change as they drag a point around a circle.
- Specify the percentages (ratios) of circumference and area for various central angles.
- Identify the connection between the central angle and the percentage of circumference and area used to determine arc length and sector area.
Vernier EasyData,Vernier EasyLink and Vernier EasyTemp are registered trademarks of Vernier Science Education.