Using Calculations in Notes

In the Notes application, the options on the Calculations menu enable you to perform calculations. The calculations are described in the following table.

Important Information to Know

• Notes does not support editing programs. Use Program Editor instead.
• Notes does not support executing Lock or Unlock commands. Use Calculator instead.
• Notes does not display intermediate results obtained using the "Disp" command. Use Calculator instead.
• Notes does not support user-defined dialog boxes obtained using the "Request," "RequestStr," or "Text" commands. Use Calculator instead.
• Notes does not support the execution of multiple statistics commands that produce stat. variables.

Menu Name

Menu Option

Function

6: Calculations

 

 

 1: Define Variables

Define a variable in a Note using the Calculator application.

 

 2: Number

Use tools from the Calculator Number menu, including Convert to Decimal, Approximate to Fraction, Factor, Least Common Multiple, Greatest Common Divisor, Remainder, Fraction Tools, Number Tools, and Complex Number Tools.

 

 3: Algebra

Use tools from the Calculator Algebra menu, including Numerical Solve, Solve System of Linear Equations, Polynomial Tools.

 

 4: Calculus

Use tools from the Calculus menu including Numerical Derivative at a Point, Numerical Definite Integral, Sum, Product, Numerical Function Minimum, and Numerical Function Maximum.

 

 3 (CAS): Algebra

Use tools from the Calculator Algebra menu, including Solve, Factor, Expand, Zeros, Numerical Solve, Solve System of Equations, Polynomial Tools, Fraction Tools, Convert Expressions, Trigonometry, Complex, and Extract.

 

 4 (CAS): Calculus

Use tools from the Calculus menu including Derivative, Derivative at a Point, Integral, Limit, Sum, Product, Function Minimum, Function Maximum, Tangent Line, Normal Line, Arc Length, Series, Differential Equation Solver, Implicit Differentiation, and Numerical Calculations

 

 5: Probability

Use tools from the Calculator Probability menu, including Factorial, Permutations, Combinations, Random, and Distributions.

 

 6: Statistics

Use tools from the Calculator Statistics menu, including Stat Calculations, Stat Results, List Math, List Operations, and others.

 

 7: Matrix & Vector

Use tools from the Calculator Matrix & Vector menu, including Create, Transpose, Determinant, Row-Echelon Form, Reduced Row-Echelon Form, Simultaneous, and others.

 

 8: Finance

Use tools from the Calculator Finance menu, including Finance Solver, TVM Functions, Amortization, Cash Flows, Interest Conversions, and Days between Dates.

 

Note: For more information, see the Calculator chapter.