Changing the Attributes of Math Expression Boxes
You can change attributes in one or more math expression boxes at the same time. Controlling the attributes in math expression boxes allows you to do the following:
|
•
|
Show or hide the input or output, or prevent calculation in the box. |
|
•
|
Select a symbol separator using Insert Symbol. |
|
•
|
Choose the number of digits to display in the output of a math expression. |
|
•
|
Select angle settings so you can use a combination of radian, degree, and gradian angle measures in the same Notes application. |
|
•
|
Select whether to allow math expressions to wrap. |
|
•
|
Select whether to show or hide warning indicators. |
To change the attributes of one or more boxes, do the following:
|
1.
|
Select the box or boxes that you want to change. |
|
3.
|
Use the menus or selection boxes to make your selections. |
|
4.
|
Click to save or to abandon the change. |
Math expression boxes recalculate automatically after you have made attribute changes and saved the changes.
Undoing Changes to Math Expression Boxes
|
▶
|
To undo changes you have made to a math expression box, press +. |