Using Math Actions

Math Actions are available on Notes, Scratchpad, and Calculator pages.

When you display the context menu for a selected expression or equation, the menu may include a Math Actions submenu that lists the available actions. Each action might prompt you for any needed parameters.

The specific math actions listed depend on:

• The type of expression or relation.
• The operating system in use (Numeric, Exact Arithmetic, or CAS).
• Any restrictions imposed by an active Press-to-Test session.

Example of Math Actions in Notes

1. Insert a math box, and type the equation x2+3x+1=0, but don't press Enter yet.

2. Display the context menu of the equation, and select Math Actions.
Windows®: Right-click the equation.
Mac®: Hold “, and click the equation.
Handheld: Point to the equation, and press / b.


Numeric and Exact Arithmetic OS


CAS OS

3. Select the action to perform:
- Solve Numerically for Numeric and Exact Arithmetic OS.
- Solve for CAS OS.

You are prompted to enter parameters. For example, Numeric Solve prompts for the variable of interest, initial guess, lower bound, and upper bound.

4. Type a value for each parameter. When options are available, you can click an arrow to make a selection.


Numeric and Exact Arithmetic OS


CAS OS

5. Click OK to construct the completed expression and place it in the math box.


Numeric and Exact Arithmetic OS


CAS OS

6. Press Enter to complete the action.


Numeric and Exact Arithmetic OS


CAS OS

7. As a further exploration, drag through the math box to select x2+3·x+1. Do not include the "=0" portion.


Numeric and Exact Arithmetic OS


CAS OS

8. Display the context menu for the selected text, select Math Actions > Find Roots of Polynomial, and press Enter to complete the action.

The action and its result are shown in a new math box.


Numeric OS


Exact Arithmetic and CAS OS

Tips for Using Math Actions in Notes

▶ For a previously evaluated expression, click in the expression and then display its context menu.

When you select an action, it replaces the expression.

▶ For a displayed result, click in the result and then display its context menu.

When you select an action, it appears in a new math box.

▶ For a portion of an expression or result, select the portion, and then display the context menu.

When you select an action, it appears in a new math box.