Activity Overview
This activity allows students to reason about ratio tables, which helps their understanding of what a ratio describes in a context and what quantities in equivalent ratios have in common.
About the Lesson
This TI-Nspire™ lesson allows students to explore the differences and similarities between ratios and fractions. Ratios are different from fractions. A ratio is a pair of non-negative numbers, a:b, which are not both 0. As one of the numbers changes, the other changes by the corresponding multiplier (i.e., if the 2 in the ratio 2:5 is changed to 6, then the 3 is changed by the same multiplier and becomes 15).
Prior to working on this lesson, students should understand:
- the concept of equivalent fractions;
- the concepts of ratios and equivalent ratios;
- how to complete ratio tables.
This is Lesson 6 out of 15 in the Building Concepts in Mathematics: Ratios and Proportional Relationships Series
Standards