About Vernier LabQuest® Sensors

You can select from a variety of Vernier LabQuest® sensors and interfaces to collect data while running the Vernier DataQuest™ application with TI-Nspire™ software.

TI-Nspire™ Lab Cradle

The TI-Nspire™ Lab Cradle lets you connect more than one LabQuest® sensor at a time.

Sensor Interface

Description

Texas Instruments TI-Nspire™ Lab Cradle

This sensor can be used with a handheld, a computer, or as a stand-alone sensor.

The sensor interface allows you to connect and use one to five sensors at the same time. It can be used in the lab or at a remote collection location.

The Lab Cradle supports two digital sensors and three analog sensors.

The Lab Cradle also supports high-sample data collection sensors, such as a hand-grip heart rate or a blood pressure monitor.

After using the Lab Cradle as a remote sensor, you can download data to either a handheld or computer.

Single-Channel Sensor Interfaces

Single-channel sensor interfaces can only connect to one sensor at a time. These sensors have either a mini-USB connector for a handheld or a standard USB connector for a computer. For a complete list of compatible sensors, see Compatible Sensors.

Sensor Interface

Description

Vernier EasyLink®

This sensor interface is used with handhelds. It has a mini-USB connector so it can be plugged directly into the handheld.

Connect sensors to Vernier EasyLink® to:

• Measure barometric pressure.
• Measure the salinity of a solution.
• Investigate the relationship between pressure and volume (Boyles’ Law).

Vernier Go!Link®

This sensor interface is used with computers. It has a standard connector so it can be plugged into a Windows® or Mac® computer.

Connect sensors to Vernier GoLink® to:

• Measure the acidity or alkalinity of a solution.
• Monitor greenhouse gases.
• Measure sound level in decibels.

Types of LabQuest® Sensors

• Analog sensors. Temperature, light, pH, and voltage sensors are analog sensors and require a sensor interface.
• Digital sensors. Photogates, radiation monitors, and drop counters are digital sensors. These sensors can only be used with the TI-Nspire™ Lab Cradle.
• Direct-connect USB sensors. These sensors connect directly to a handheld or computer and do not require a sensor interface.

Sensors for Handhelds

The following lists some sensors you can use with a handheld.

Sensor

Description

Texas Instruments CBR 2™

This analog sensor connects directly to TI-Nspire™ CX II handhelds through the mini-USB port. It is used to explore and graph motion.

This sensor automatically launches the Vernier DataQuest™ application when you connect it to a handheld. Data collection begins when you select the Motion Match function.

This sensor collects up to 200 samples per second.

Use this sensor to:

• Measure position and speed of a person or object.
• Measure the acceleration of an object.

Vernier EasyTemp® temperature sensor

This analog sensor connects directly to TI-Nspire™ CX II handhelds through the mini-USB port and is used to collect temperature ranges. You can design experiments to:

• Collect weather data.
• Record temperature changes due to chemical reactions.
• Perform heat fusion studies.

Sensors for Computers

The following table lists some sensors you can use with a computer.

Sensor

Description

Vernier Go!Temp® temperature sensor

This analog sensor connects to the computer’s USB port and is used to collect temperature ranges.

You can use this sensor to:

• Collect weather data.
• Record temperature changes due to chemical reactions.
• Perform heat fusion studies.

Vernier Go!Motion® motion detector

This analog sensor connects to the computer’s USB port and is used to measure acceleration, speed, and velocity.

Use this sensor to:

• Measure position and speed of a person or object.
• Measure the acceleration of an object.

Compatible LabQuest® Sensors

The following sensors can be used with the Vernier DataQuest™ application.

• 25-g Accelerometer
• 30-Volt Voltage Probe
• 3-Axis Accelerometer
• Low-g Accelerometer
• CBR 2™ - Connects directly to handheld USB port
• Go!Motion® - Connects directly to computer USB port
• Extra Long Temperature Probe
• Stainless Steel Temperature Probe
• Surface Temperature Sensor
• Ammonium Ion-Selective Electrode
• Anemometer
• Barometer
• Blood Pressure Sensor
• C02 Gas Sensor
• Calcium Ion-Selective Electrode
• Charge Sensor
• Chloride Ion-Selective Electrode
• Colorimeter
• Conductivity Probe
• High Current Sensor
• Current Probe
• Differential Voltage Probe
• Digital Radiation Monitor
• Dissolved Oxygen Sensor
• Dual-Range Force Sensor
• EasyTemp® - Connects directly to handheld USB port
• EKG Sensor
• Electrode Amplifier
• Flow Rate Sensor
• Force Plate
• Gas Pressure Sensor
• Go!Temp® - Connects directly to computer USB port
• Hand Dynamometer
• Hand-Grip Heart Rate Monitor
• Instrumentation Amplifier
• Light Sensor
• Magnetic Field Sensor
• Melt Station
• Microphone
• Nitrate Ion-Selective Electrode
• O2 Gas Sensor
• ORP Sensor
• pH Sensor
• Relative Humidity Sensor
• Respiration Monitor Belt (Requires Gas Pressure Sensor)
• Rotary Motion Sensor
• Salinity Sensor
• Soil Moisture Sensor
• Sound Level Meter
• Spirometer
• Thermocouple
• TI-Light - Sold only with the CBL 2™
• TI-Temp - Sold only with the CBL 2™
• TI-Voltage - Sold only with the CBL 2™
• Tris-Compatible Flat pH Sensor
• Turbidity Sensor
• UVA Sensor
• UVB Sensor
• Vernier Constant Current System
• Vernier Drop Counter
• Vernier Infrared Thermometer
• Vernier Motion Detector
• Vernier Photogate
• Voltage Probe
• Wide-Range Temperature Probe