Using Data Markers to Annotate Data
Data markers give you a way to emphasize specific data points, such as when you change a condition. For example, you might mark a point at which a chemical is added to a solution or when heat is applied or removed. You can add a marker with or without a comment, and you can hide a comment.
Two data markers, one with a comment displayed
Marker shown as red triangle in Table view
| ▶ | Click Add Data Marker |
| 1. | In Graph or Table view, click the point at which you want a marker. |
| 2. | Click Add Data Marker |
| 3. | Complete the items in the dialog box. |
| 1. | In the Detail view, click to expand the list of markers for the data set. |
| 2. | Click the entry for the marker that you want to change, and complete the items in the dialog box. |
| 1. | Click to expand the list of markers in the Detail view. |
| 2. | Click the entry for the marker that you want to change. |
| 3. | In the dialog box, type a new value for Mark Value at. |
| ▶ | Drag the comment to move it. The connecting line remains attached to the data point. |
| ▶ | Hide a comment by clicking the X at the end of the comment. |
| ▶ | To restore a hidden comment: |
| a) | Click to expand the list of markers in the Detail view. |
| b) | Click the entry for the marker that you want to change, and check Show Comment on Graph. |
| 1. | Click to expand the list of markers in the Detail view. |
| 2. | In the dialog box, click Remove. |