Education Technology

Expressions and Equations / Building Expressions

Grade Level 6
Activity 3 of 18
In this lesson students focus on comparing expressions and establish a foundation for the definition of equivalent expressions.

Planning and Resources

Objectives
Students should identify equivalent expressions and explain why they are equivalent using properties of multiplication and addition. They use a variety of strategies, including rewriting an expression and properties of operations, to develop equivalent expressions.

Vocabulary
expression
variable
constant
associative property
commutative property
distributive property
equivalent expressions


Standard: Search Standards Alignment

Downloads

Lesson Snapshot

Understanding

Two expressions are equivalent if they have the same value for every possible replacement for the variable or variables.

What to look for

Some statements can be true for many values of a variable or variables but not true for others. For example, “multiplication” makes things larger is true if you are multiplying whole numbers greater than 1.

Sample Assessment

Which expression is equivalent to 8(x-2) + 4(3-x) - 2x?

Answer: 2x-4

The Big Idea

Students consider how to verify that expressions are equivalent by using the associative and commutative properties of addition and multiplication as well as the distributive property.

What are the students doing?

Students reason about values produced by an expression as the variable x changes and look for relationships between the structure of the expression and its value.

What is the teacher doing?

Engage students in reasoning about the values produced by an expression as the variable x changes and in looking for patterns and relationships between the structure of the expression and its value.