Education Technology


Integers! It All Adds Up!

Activity Overview

Students use the number line to investigate how to add integers and to justify and support the rules that they develop.

Key Steps

  • Image

    In this activity, students will use the Number Line application to investigate adding positive and negative integers. For the first problem, students will add only positive integers. They are introduced to the concept of "number rays" or vectors to represent the operation of addition.

  • Image

    In the second problem students will add only negative integers. They will also investigate adding a negative integer and a positive integer. Lastly, students see how opposite integers always have a sum of 0.

  • Image

    After determining patterns for the addition of integers, students are encouraged to develop mental arithmetic strategies and practice using them with the additional problems given on the worksheet.