Find answers to the top 10 questions parents ask about TI graphing calculators.
Download free 90-day trial versions of the most popular TI software and handheld emulators.
Learn about the math and science behind what students are into, from art to fashion and more.
Get ready for back to school with T³™ Webinars to enhance your teaching and TI technology skills.
Get hundreds of video lessons that show how to graph parent functions and transformations.
Update OS, transfer files andtake screen captures for yourTI-Nspire™ CX II graphing calculator.
Texas Instruments
9-12
15 Minutes
TI Connect™TI Connect™ CE
Students will explore the definition of a function through use of a graph, a set of ordered pairs, and an input-output diagram.
In the first problem, students will explore a position-vs.-time graph. After being introduced to the definition of a function, they will determine if the graph is a function of time, then update the graph to show a function.
Then students will calculate the output values for given input values using the distance formula d = 0.5at2 for when a = 12 ft/s2. The first set of input values are for t and the second set of input values are for d.
Students will then explore using function notation on the calculator entering input values to find the output value. The given function is stored in the Y= screen.
In the last problem, students will use the program MACHINE which acts like a function machine. When they enter an input value, it will return the output value. They are to determine the input value for the goal output and the mystery function.
TI websites use cookies to optimize site functionality and improve your experience. To find out more or to change your preferences, see our cookie policy page. Click Agree and Proceed to accept cookies and enter the site.
You can control your preferences for how we use cookies to collect and use information while you're on TI websites by adjusting the status of these categories.