Activity Overview
This activity allows students to explore situations in which points with a constant sum of x-coordinate and y-coordinate are graphed. Through the use of TI-Navigator to see the results of the entire class, students can determine that an oblique line is formed from such points. This oblique line always has intercepts equal to the constant sum. The Learning Check enables the teacher to get immediate feedback from the students, thus giving opportunities to correct any errors in understanding.
Before the Activity
Before the Activity create a Learning Check that has the questions:
If a line has points for which the sum of the x-coordinate and the y-coordinate is 11, what kind of line is it?
Horizontal
Oblique
Vertical
If a line has points for which the sum of the x-coordinate and the y-coordinate is 11, its graph has an x-intercept of ____ and a y-intercept of ____.
If a line has points for which the sum of the x-coordinate and the y-coordinate is 11, its graph passes through which quadrant(s)?
Quadrant 1
Quadrant 2
Quadrant 3
Quadrant 4
Start TI-Navigator and begin the class.
During the Activity
See the attachment
After the Activity
Send a Learning Check file to the class to check for their understanding. The first question is a multiple choice one.
If a line has points for which the sum of the x-coordinate and the y-coordinate is 11, what kind of line is it?
Horizontal
Oblique
Vertical
The second question is a fill-in-the-blank type.
If a line has points for which the sum of the x-coordinate and the y-coordinate is 11, its graph has an x-intercept of ____ and a y-intercept of ____.
The third question is a multiple choice one for which there is more than one correct answer.
If a line has points for which the sum of the x-coordinate and the y-coordinate is 11, its graph passes through which quadrant(s)?
Quadrant 1
Quadrant 2
Quadrant 3
Quadrant 4
Collect the answer files from the classroom. Display the slide show of student responses and discuss the results.