Education Technology


VIC: Eye Spy

by Texas Instruments

Objectives

Use calculus to determine the maximum area of a circle that just fits inside another curve. The combined curves appear as an eye adding some visual interest to the problem. The activity also introduces some techniques that students may use to help solve other, more complicated problems. 

Vocabulary

  • Differential Calculus
  • Exponential function
  • Gradient of a function
  • Substitution (algebra)
  • Simultaneous equations

About the Lesson

The calculus in this activity is relatively straight forward, however students need to be careful. There are several approaches to solving this problem and almost as many ways to overlook simple assumptions. It is a necessary condition that the gradient of the two curves (iris and eye boundary) are the same where the maximum iris area occurs, but these are not sufficient conditions. An accurate and animated visual help solve the problem as well as introducing some straight forward techniques. With or without CAS, the algebra and calculus in this problem is readily accessible.