Education Technology

Unit 1 includes geometry, combinatorics and vectors. Geometry extends students’ studies in Euclidean Geometry, knowledge which is of great benefit in the later study of topics such as vectors and complex numbers. Combinatorics incorporates techniques applicable to probability and algebra and vectors in the plane provides new perspectives on working with two-dimensional space.

Unit 2 includes trigonometry, matrices, real and complex numbers. Matrices provide new perspectives for working with two-dimensional space, real and complex numbers provides a continuation of the study of numbers and trigonometry contains techniques that are used in other topics in both this unit and Units 3 and 4.