Saving Screens When Using Capture Class

You can save captured screens for use in other TI-Nspire™ documents that allow images or for use in another application such as Microsoft® Word. You can save images in the following formats: .jpg, .png, or .gif. You can save one image at a time, select multiple images to save, or save all captured images.

Saving Screen Images

To save screen images captured when using Capture Class, complete the following steps.

1. In the Class Screen Capture window, select the screen or screens you want to save as image files.
• To select multiple consecutive screens, click the first image, and then hold down the Shift key and click the additional images. To select screens in random order, hold down the Ctrl key (Mac®: “) and click each image you want to save.
• To select all captured screens, click Edit > Select All.
2. Click File > Save Selected Screen(s) or press Ctrl + S (Mac®: “ + S).

The Save dialog box opens.

3. Navigate to the folder on your computer where you want to save the file(s).
4. Type a name for the file or files in the File Name field.

The default file name is Image.

5. In the Files of Type field, click ¤, and then select the file type: .png, .jpg, or .gif. The default file type is .jpg.
6. Click Save.

The file or files are saved in the designated folder.

• If you saved one image, the file is saved with the name as specified in the File Name field.
• If you saved multiple images, the files are saved with the name specified in the File Name field with a number appended to the file name to make each file name unique. For example, Image1, Image 2, and so on.