Saving Captured Pages and Screens
You can save captured pages and screens captured as images for use in other TI-Nspire™ documents that allow images or for use in other applications such as Microsoft® Word. You can save one image at a time, select multiple images to save, or save all captured images.
| 1. | In the Screen Capture window, select the screen image you want to save. |
| 2. | Click File > Save Selected Screen(s). |
Note: From the Screen Capture window, you can also click
.
The Save as dialog box opens.
| 3. | Navigate to the folder on your computer where you want to save the file. |
| 4. | Type a name for the file. |
Note: The default file name is MM-DD-YYYY Image ###.
| 5. | Select the file type for the image file. The default format is .jpg. Click ¤ to select another format: .gif, .tif, or .png. |
| 6. | Click Save. |
The file is saved in the designated folder.
| 1. | In the Screen Capture window, select the screens you want to save. |
To select multiple consecutive screens, click the first image, and then hold down the Shift key and click the additional images. To select screens in random order, press Ctrl (Mac®: “) and click each image you want to save.
| 2. | Click |
Note: The "Save All Screens" option is not available when using Capture Class.
The Save as dialog box opens.
| 3. | In the Save In field, navigate to the folder where you want to save the images. |
| 4. | In the File Name field, type a new folder name. The default folder name is MM-DD-YYYY Image, where MM-DD-YYYY is the current date. |
| 5. | Select the file type for the image files. The default format is .jpg. Click ¤ to select another format: .gif, .tif, or .png. |
| 6. | Click Save. |
The images are saved in the specified folder with system-assigned names reflecting the current date and a sequence number. For example, MM-DD-YYYY Image 001.jpg, MM-DD-YYYY Image 002.jpg and so on.