Education Technology

Units 1 & 2 provide an introductory study of simple elementary functions of a single real variable, algebra, calculus, probability and statistics and their applications in a variety of practical and theoretical contexts. The focus of Unit 1 is the study of simple algebraic functions. Unit 2 students focus on the study of simple transcendental functions and the calculus of simple algebraic functions. The areas of study covered in each unit include Functions and Graphs, Algebra, Calculus, Probability and Statistics. For more information on the Mathematical Methods course visit the VCAA website.

VIC: Mathematical Methods Yr11 Classroom ActivitiesDownload
Calculus

Gradient of a function

This activity introduces the notion of the gradient of a curve. Initial exploration involves a dynamic tangent where students can use prior knowledge of the gradient of a straight line to determine if the slope is negative, zero or positive. The second stage of the activity goes one step further by quantifying the gradient. The third stage sees the gradient function generated automatically including an opportunity to freely explore the relationship between a parabola and its gradient function. T
Download100

A Special Function

Finding the derivative of a polynomial is relatively straight forward, but what about other functions? This activity explores a function with a special property; “the derivative of the function is the same as the original function”! The problem is initially explored using a dynamic line where changes to the line immediately affect the derivative of the line. Manipulating this line provides for instant feedback helping students determine the likely shape of such a function. Calculations involvin
Download58

Take it to the limit

Students explore how a regular polygon can be used to approximate the perimeter and area of a circle. The purpose of the activity is to provide a practical, geometric approach to understanding the concept of a limit.
Download56
/media library/Images/Activities/AUS-NZ/Missing Image Default

Triangle Areas

A triangle circumscribes a rectangle. The triangle is not unique, so what is the minimum area of the triangle that circumscribes the triangle? Students use the dynamic representation on TI-Nspire, data capture and more to explore this problem with some elegant solutions. 
Download10

Fill the Vase

Students interpret graphs of empirical data with respect to rate of change of the height of water in vases of different shapes that are being filled at a constant rate. Students are provided with a range of graphs and vases. For each graph they must reshape the vase in order to match the volume – height graph. For each vase they must produce a volume – height graph. Practical ideas including data collection and videos are provided in the teacher notes.
Download103
Paper Folding Thumb

Paper Folding

In this activity students maximize the area of a triangle formed when a piece of A4 paper is folded in a special way. The activity provides an opportunity to explore the problem practically followed by an animated TI-Nspire file that automatically generates data so that students are able to check the validity of their data before proceeding. The unusual general result from this task makes the activity quite intriguing.
Download64
Ladder Problem Thumb

Ladder Problem

Maddi the painter needs to work out the longest ladder that she can get around a tight hallway corner. Formulate an expression for the length of the ladder, differentiate and make equal to zero. Then what? Why does the function minimum align with the longest ladder?

Download38
Eye Spy

Eye Spy

Students use calculus to determine the maximum size of the iris (circle) that just fits inside an outline of the eye defined by two bell shaped curves. The activity uses some basic differential calculus, introduces simple substitutions to eliminate variables and handy techniques for simplifying problems. The problem is much easier than it looks!
Download12