Browse Activities | TI-84 Plus Family - High School

ccss-act-week6-84c-alg1-small

Perms and Combs?

Students will use built-in commands to evaluate factorials, combinations, and permutations.

ccss-act-week6-84c-alg1-small

Spreading Doom

Students explore a geometric sequence that models the spread of a computer virus.

Binomial Probabilities

Students will simulate rolling a die and keeping track of the numbers of successes and failures.

Modeling Data

Students will graph data modeling exponential and logarithmic growth and find equations representing the data.

Quadratric Regression with Transformation Graphing

Students will compare the data plots and different regression models for a set of data. Students will also learn to draw conclusions using the quadratic model.

Constructing with Similar Triangles

Students will investigate three different methods of constructing similar triangles.

Transformational Puppet

Students will construct a puppet using line segments and circles and transformations and then manipulate their puppet to see the effect of changes.

Circle Product Theorems

Students will use dynamic models to find patterns. These patterns are the Chord-Chord, Secant-Secant, and Secant-Tangent Theorems.

Running Circles Around Quads

Students will explore various properties of cyclic quadrilaterals.

Angles & Arcs

Student will explore angles constructed in a circle and how their measures are related to the measures of the intercepted arcs.

Exploring Cavalieri's Principle

Students will explore Cavalieri's Principle for cross sectional area and volume.

Distances in the Coordinate Plane

Students will explore distances in the coordinate plane. After finding the coordinates of a segment’s endpoints, students will substitute these values into the distance formula and compare the results to the measured length of the segment.

The Geometric Mean

Students will discover that triangles are similar and then determine the altitude of the hypotenuse of a right triangle.

Properties of Parallelograms

Students explore the various properties of parallelograms and the necessary and sufficient conditions that guarantee that a quadrilateral is a parallelogram.

Special Segments in Triangles

Students will construct and explore medians, altitudes, angle bisectors, and perpendicular bisectors of triangles.

Interior & Exterior Angles of a Triangle

Students measure interior and exterior angles of a triangle and make conjectures about their relationships.

Triangle Sides & Angles

Students will explore side and angle relationships in a triangle and determine the number of acute, right, or obtuse angles that can exist in any one triangle.

Parallel Lines Cut by a Transversal

Students use measurement tools to develop and strengthen their knowledge about the angles formed when parallel lines are cut by a transversal.

Vertical and Adjacent Angles

Students make conjectures about relationships of angle pairs by exploring vertical and adjacent angles in a model.

Conditional Statements

Students explore slopes of parallel and perpendicular lines and use evidence to justify or counterexamples to disprove logical statements.

Diameter and Circumference of a Circle

In this activity, students explore the relationship between a circle's circumference and its diameter. This will lead students to their own discovery of a value for pi.

ccss-act-week6-84c-alg1-small

Inverse Variation

Students explore the inverse variation function with a geometric representation (a rectangle with fixed area), a table of values, an algebraic expression, and a graph.c

ccss-act-week6-84c-alg1-small

Stop!

Students will use an interactive page to calculate the speed of the car, given a stopping distance, and then approximate stopping distance, given the rate of the car.

ccss-act-week13-84c-alg1-small

Graphing Quadratic Functions

Students will explore the inverse variation function with a geometric representation (a rectangle with fixed area), a table of values, an algebraic expression, and a graph.

ccss-act-week6-84c-alg1-small

Introducing the Parabola

Students will plot the points from the table and examine the graph and its properties.

ccss-act-week6-84c-alg1-small

Quadratic Formula

Students will make connections between the visual ways to find zeros of a parabola and algebraic ways with an emphasis on the quadratic formula.

ccss-act-week6-84c-alg1-small

Exponent Rules

Students will discover rules for working with exponents, such as the Power of a Power rule and investigate the value of a power whose exponent is zero or negative.

ccss-act-week6-84c-alg1-small

Going Into Business

Students will translate fixed and variable costs of a cost function and make a decision about how much to charge to wash per dog.

ccss-act-week6-84c-alg1-small

Chirp, Jump, Scatter

Students will find a best fit line for data graphed as scatter plots.

ccss-act-week6-84c-alg1-small

Trains in Motion

Students will make observations about the motion of two objects. They will compare and contrast this motion and consider how it corresponds to a graph representing distance as a function of time.

ccss-act-week4-84c-algebra-1-small

Back In Time?

Students will explore the definition of a function through use of a graph, a set of ordered pairs, and an input-output diagram.

ccss-act-week4-84c-algebra-1-small

Supertall Skyscrapers

Students use scaled measurements and proportions to find the heights of skyscrapers.

Linear Inequalities

Students investigate single-variable inequalities on a number line and as a table of values.

One Step at a Time

Students use repeated results from calculations to formulate and test a hypothesis about solving one-step equations.

Raise Your Cup

Students will explore writing and graphing inequalities. Students will solve inequalities to determine the height for a cup that needs to hold at least 12 ounces. They will use a trial and error method, entering values into the table to compute their range of answers.

Areas in Intervals

Students will estimate and find a given area under a normal curve.

Vertical and Phase shifts

Students will explore vertical and phase shifts of sine and cosine functions.

Exponential Reflections

Students will determine that the inverse of the exponential function is the natural log function by plotting the inverse of exponential solution points.

Exponential Growth

Students will find an approximation for the value of the mathematical constant e and to apply it to exponential growth and decay problems.

Geometric Sequences & Series

Students will find common ratios of geometric sequences on a spreadsheet and create scatter plots of the sequences to see how each curve is related to the value of the common ratio.

Stacking Bricks

Students will use a polynomial function to model a real world problem.

Border Patrol

Students will graph a system of linear inequalities to determine if a points lies in the solution.

Roots of Radical Equations

Students will solve square root and cube root equations graphically.

Watch Your P's and Q's

Students will then use the Rational Zero Theorem to find all the potential rational zeros of the function.

Just Move it

Students explore transformations of parent functions by comparing changes in the equations to their graphs.

Airport Impact Study

Students develop a model to analyze and explain data collected in an airport noise impact study.

Area of the Missing Square

Students will use an area model to represent and explore patterns in the structure of the quadratic equation.

Operating on Matrices

Students will perform operations on matrices. Using teacher discussion questions, students can determine the row and column properties of matrices to conclude when the operations can be performed.