Starting a Transfer

After you have added all files and folders to the Transfer List and selected other options as necessary, you can start the transfer. You can transfer operating system files and documents at the same time.

To start a transfer:

1. Connect one or more TI-Nspire™ handhelds.

If handhelds are not connected, the Status tab indicates “No Active Connected Handhelds” when you start a transfer.

2. From the Resources pane, complete one of the following actions:
• To transfer files to one or more TI-Nspire™ handhelds, select the individual handhelds.
• To transfer files to all connected TI-Nspire™ handhelds, select Connected Handhelds (top level).
3. In the Transfer Tool dialog box, click Start Transfer.

The Transfer Tool dialog box switches to the Status tab and displays the transfer information.

• The progress bar disappears when a transfer is complete.
• During a transfer, the Transfer Tool indicates which handhelds are connected and successfully received files.
• If a handheld disconnects and then reconnects during a transfer, the Transfer Tool indicates the status of completed transfers, and resumes transferring other files as necessary.