Changing TI-SmartView™ Options

You can change the emulator options, even when the emulator panel is closed.

1. In the teacher software, click File > Settings > TI-SmartView™ Options.

The TI-SmartView™ Options dialog box opens.

In the student software, click File > Settings > Keypad Options.

The Keypad Options dialog box opens.

2. Click Browse to change the folder where documents are saved and accessed in the My Documents folder when using the emulator.

Important: If you change the TI-SmartView™ location, you must also copy or move the MyLib folder and paste it to the new location to see library objects.

The default location of MyLib is:

• Windows®: Documents\TI-Nspire\MyLib.
• Mac®: Documents/TI-Nspire/MyLib.

Note: Close and reopen the TI-Nspire™ application for the libraries to reflect the change.

3. Click ¤ to open the menu and select a faceplate.
4. In the teacher software, click ¤ to open the menu and select a view. If selecting Handheld Only, select Always in Front to keep this window on top of all other open applications.
5. Click OK to save the settings.