| Module 11 - Extreme Values and Optimization | |||||||||||||
| Introduction | Lesson 1 | Lesson 2 | Lesson 3 | Lesson 4 | Self-Test | |||||||||||||
| Lesson 11.3: The Can Problem | |||||||||||||
|
In Lesson 11.2 the length of a removed arc that maximized the volume of a cone was found. In this lesson the radius of a can that minimizes surface area will be explored.
Stating the Problem A right cylindrical can is being designed to hold 255 cubic units. Find the radius of the can with the least surface area and find the minimum surface area. Drawing the Diagram The diagram below illustrates a can of radius r and height h.
Finding Surface Area as a Function of r and h
The quantity to be minimized is surface area. The surface area includes the lateral surface formed by a rectangle with height h and width 2
Defining r and h as Functions of x The surface area is a function of two variables, r and h. If r and h are both defined in terms of a single variable x, then the surface area will be defined as a function of x, which will allow it to be graphed on the TI-89. Writing h and r as Functions of x
The desired volume is 255 cubic units and the formula for volume is V =
Solving the equation for h gives
Letting r = x, r and h can be defined as functions of x.
Now we have surface area s(x), completely defined as a function of x, as shown in the following screen.
Finding the Derivative of Surface Area with respect to x Store the derivative of the surface area, s, in a new function named ds.
Alternatively, we could compute the derivative of s(x) directly from the formula found in the previous figure. Finding the Zero(s) of the Derivative Because the radius of the can must be greater than zero, the domain of the surface area function is all x > 0. Notice that if r = k is very large, then h is very small. Find the exact value and the approximate value of the zero of the derivative.
Checking for Other Possible Extreme Values
The first derivative is defined everywhere in the function's domain, so x
Using the Second Derivative The second derivative can often be used to determine if a critical point where the first derivative is zero indicates a local maximum or a minimum by revealing the function's concavity at that point. No conclusion can be drawn if the second derivative is zero or undefined at the critical point. The table below summarizes the relationship.
Test the critical point in the second derivative of the surface area function to determine whether it represents a local minimum. Use the exact value from the history screen.
Because the second derivative of the surface area function is positive at x = 3.43653, the graph of the function is concave upward and has a local minimum value there. Because there are no endpoints and no other critical points, the local minimum value is the absolute minimum value. Finding the Minimum Surface Area Find the minimum surface area of the can by evaluating s(x) with the exact x-value that minimizes surface area. Then get the approximate value of the minimum surface area.
The minimum surface area of a cylindrical can that holds 255 cubic units is approximately 222.61 square units. The radius which will result in the minimum surface area is approximately 3.43653 units. Graphing the Surface Area Function and Its First Derivative As shown in Lesson 11.2, the graphs of the function and its first derivative illustrate the relationship between the function's minimum value and the corresponding zero of its derivative. 11.3.1
Click here for the answer. Generalizing and Extending the Can Problem The problem can be generalized by replacing the fixed volume of 255 with a letter and proceeding as in the last example. The problem can be further extended by exploring the ratio of height to radius for a right cylindrical can with fixed volume that has minimum surface area. Replacing 255 with v The first occurrence of the fixed value of the volume appears in the function that represents the height of the can. Replace the volume of the can with the letter "v" and redefine the function.
Finding The Zero(s) of the Derivative Determine when the derivative is zero.
This value of x is the radius which will result in the minimum surface area.
The corresponding value of the minimum surface area is s = 3(2
Finding the Ratio
Evaluate the ratio of height to radius,
Paste the last part of the command from the History Area.
The ratio of height to radius is 2, regardless of the volume v. That is, for right cylindrical cans with a fixed volume, when the height of the can is twice the radius the surface area of the can will be minimized. |
|||||||||||||
| < Back | Next > | |||||||||||||
|
©Copyright
2007 All rights reserved. |
Trademarks
|
Privacy Policy
|
Link Policy
|