| Module 7 - Velocity | ||||||||||||||||||||||||||||||||||||
| Introduction | Lesson 1 | Lesson 2 | Lesson 3 | Self-Test | ||||||||||||||||||||||||||||||||||||
| Lesson 7.2: Instantaneous Velocity | ||||||||||||||||||||||||||||||||||||
|
In Lesson 7.1 you found average velocities over different time intervals. In this lesson you will find the instantaneous velocity of the falling object at t = 0.16. Each of the average velocities found in Lesson 7.1 could be considered an approximation of the instantaneous velocity at t = 0.16, but none was exact. Getting Better Approximations You can use the average velocity function you defined in Lesson 7.1 to find a series of approximations that will lead to the instantaneous velocity of an object at a given instant. 7.2.1 Use the function avel you defined in Lesson 7.1 to enter the average velocities over the intervals near t = 0.16 indicated by the following data points, and use DrawSlp to draw the corresponding lines on the scatter plot. Click here for the answer.
7.2.2 Which of the three average velocities is the best approximation to the instantaneous velocity? Why? Click here for the answer.
Fitting a Curve to the Data
The smaller the elapsed time interval, the better the average velocity approximates the instantaneous velocity. The smallest interval near t = 0.16 provided by the data is 0.02. However, if you could find a continuous curve through the scatter plot, you could find points on the curve even closer to
Using the Regression Equation
The height of the book at t = 0.16 and t = 0.18 can now be approximated by finding y1(0.18) and
This result is a good approximation of the average velocity of -1.75 you found in Question 7.2.2 using the table data values over the same interval. Finding Even Better Approximations Points even closer to (0.16, 0.716) may be found by using the quadratic function stored in y1. Find the average velocity for the interval from t = 0.16 and t = 0.17.
7.2.3 Using the regression equation in y1, find the average velocities for the following smaller and smaller time intervals. t = 0.16 to t = 0.161 (elapsed time = 0.001 seconds) t = 0.16 to t = 0.1601 (elapsed time = 0.0001 seconds) t = 0.16 to t = 0.16001 (elapsed time =0 .00001 seconds) Click here for the answer. Finding Instantaneous Velocity
As the elapsed time approaches zero, the average velocities approach a limiting value. This limit is the instantaneous velocity, which can be found by letting h represent the elapsed time and evaluating
The instantaneous velocity at t = 0.16 is 1.6496 m/s.
Visualizing Instantaneous Velocity A special line is associated with the instantaneous velocity.
The line is
|
||||||||||||||||||||||||||||||||||||
| < Back | Next > | ||||||||||||||||||||||||||||||||||||
|
©Copyright
2007 All rights reserved. |
Trademarks
|
Privacy Policy
|
Link Policy
|
||||||||||||||||||||||||||||||||||||