| Module 7 - Velocity | ||||||||||||||||||||||||||||||||||||||||||||
| Introduction | Lesson 1 | Lesson 2 | Lesson 3 | Self-Test | ||||||||||||||||||||||||||||||||||||||||||||
| Lesson 7.1: Average Velocity | ||||||||||||||||||||||||||||||||||||||||||||
|
In this lesson you will define a function that will be used to find average velocities of a falling object. You will use this function to calculate and compare average velocities over several different time intervals and then illustrate these velocities. Dropping a Book A book was dropped from a height of 0.865 meters. Its height above ground was monitored with a Texas Instruments Calculator-Based Laboratory (CBL). The following table contains data of the book's height in meters versus time in seconds.
Click here to review the Keystrokes to enter the data. Click here to review the Keystrokes to create a scatter plot.
The Window shown is [-0.028, 0.308] x [0.4129, 0.9061] with xscl = 0.014 and yscl = 0.02055. Calculating Average Velocity Average velocity is defined to be the change in position divided by elapsed time. If h1 is the height at time t1 and h2 is the height at time t2, h2 h1 represents change in position, t2 t1 represents elapsed time, and
Defining a Function of Several Variables The TI-89 calculator can define a function that will compute average velocity using the four values t1, h1, t2 and h2.
The function avel will return the average velocity between the two points (t1, h1) and (t2, h2). Finding the Average Velocity over t = 0 to t = 0.28 Use the function avel to find the average velocity from (0, 0.865) to (0.28, 0.454).
The average velocity over the interval from t = 0 to t = 0.28 was approximately 1.468 m/sec. The negative sign means the object is moving downward. Finding the Average Velocity over Subintervals 7.1.1 Find the average velocity for
Click here for the answer. 7.1.2 The second average velocity has a larger magnitude than the first. What does this tell you about the falling object? Click here for the answer. Average Velocity as Slope The average velocity from (0, 0.865) to (0.28, 0.454) is also the slope of the line through the corresponding points on the scatter plot. You can graph this line with the DrawSlp (Draw Slope) command, which is found in the catalog. It requires the coordinates of a point (x, y) and a slope m, and its syntax is Because average velocity is also the slope, you can use the previous result as the desired slope.
Notice there are no parentheses in this command.
The slope of this line is the average velocity for the entire interval given in the table. Illustrating Slopes of Subintervals The average velocity of the book during the subinterval from t = 0 to t = 0.16 can be illustrated by drawing the line that contains the points (0, 0.865) and (0.16, 0.716).
Finally, draw the line associated with the average velocity from (0.16, 0.716) to (0.28, 0.454).
The slope of each line is equal to an average velocity over an interval.
Press
|
||||||||||||||||||||||||||||||||||||||||||||
| < Back | Next > | ||||||||||||||||||||||||||||||||||||||||||||
|
©Copyright
2007 All rights reserved. |
Trademarks
|
Privacy Policy
|
Link Policy
|
||||||||||||||||||||||||||||||||||||||||||||